AnsweredAssumed Answered

How to prevent the L298 from heating?

Question asked by godse.akshay on Feb 3, 2017
Latest reply on Feb 3, 2017 by Enrico Poli

Hello, I am using L298N motor driver in parallel mode.But while running the motor L298N IC heats too much and suddenly stop. Motor specification are as follows:- Voltage=12V, Stall current=50A, Rated current=5A. Can

Motor specification are as follows:- Voltage=12V, Stall current=50A, Rated current=5A. Can I use Sense resistor for current limiting? If yes then how do I calculate the value of Rs?

Please help me.

Outcomes