AnsweredAssumed Answered

STM32L051 and VREF out

Question asked by Siloret.Lauret on Feb 3, 2017
Latest reply on Feb 3, 2017 by Jocelyn RICARD

Hello,

I selected the STM32L051C6T6 for a small project (package LQFP32)

The datasheet states that this microcontroller has a VREFint out pin (PB1, additionnal functions).

 

I just can't find out how to output the internal analog reference voltage on this pin. There is absolutely no piece of information on how to do this on the datasheets.

 

I enabled the VREFINT bit in ADC_CCR register (I can actyally read the Vref value with the ADC), I tried differents MODER settings for the GPIOB (alternate mode, analog mode), had a look into PWR_CSR register and the VREFIN
TRDYF is 1.

 

But still no 1.224V on the output.

 

Does anyone have an idea ?

Thanks,

Outcomes