AnsweredAssumed Answered

STM32Cube doesnt allow HARD_INPUT for SPI slave

Question asked by g.c.003 on Feb 1, 2017

Setting up SPI1 as a slave using STM32CubeMx 4.19.0

On the pinout tab of STM32Cube, I can configure SPI1 as Full-Duplex Slave and choose HardwareNSS_Input 

 

But on the configuration tab , selecting SPI1 configuration , there is a pull down for  "NSS Signal Type" that only allows me to select "Software" and not "Hard_Input"

 

The code that is generated sets it to SPI_NSS_SOFT

 

Is the tool broken or did I miss some configuration?

I think this worked correctly back in 4.13

Outcomes