AnsweredAssumed Answered

SPWF01: Module enters IP 192.168.0.50

Question asked by Flow on Jan 30, 2017
Latest reply on Feb 1, 2017 by Gerardo Gallucci

Hi,

my modules are sometimes returning the IP address 192.168.0.50 since they already had another IP address from the access point. When they got the IP address 192.168.0.50, I can't connect to them via TCP anymore. Then I have to reset the device.

Does anyone has this behavior, too? Or has an idea why the modules change it's IP address?

 

Regards,

Flow

Outcomes