AnsweredAssumed Answered

[CubeMX feature request]Please add an user section after the HAL_Init()

Question asked by marton.miklos on Jan 27, 2017
Latest reply on Sep 15, 2017 by marton.miklos

Dear STM32 Cube MX developers!

 

I am facing with the following problem, and I have not been able to find a proper solution:

 

I am using a STM32F103 with CDC stack via USB.

I have to add a code snippet to force the re-enumeration between the debug sessions.

 

Here is the generated code:

 

 
  /* USER CODE BEGIN 1 */
  uint8_t i, checksum;
  /* USER CODE END 1 */

  /* MCU Configuration----------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* Configure the system clock */
  SystemClock_Config();

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART1_UART_Init();
  MX_USB_DEVICE_Init();

  /* USER CODE BEGIN 2 */
  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
*/

I need to add my code after the 

 

SystemClock_Config();

but before the

MX_USB_DEVICE_Init();

 

I have not found any user generated sections between these two sections.

Outcomes