AnsweredAssumed Answered

ADC triger on PWM edge

Question asked by anton.bogdan on Jan 25, 2017
Latest reply on Jan 26, 2017 by anton.bogdan

Hello,

 

On a STM32F407VE device   i have a timer2 which reads 3 hall sensors from a bldc motor,  this timer is feeding the trigger signal into a advanced timer1 which generates 6pwm's for the transistor bridge.

 

The  reading of the hall sensors and the comutation step configs,  are made inside  the timer2 cc1 irq handler.

 

The FET signals are TIM_OCMode_PWM1 for high side channels ( CH1, CH2,CH3)    and for low side channel ( CH1N, CH2N, CH3N) its just regular low/high state  

 

Till here everything is ok, the signals have the corect phase

 

 

But i was thinking to ad a current measurement feature  using one ADC channel ( ADC_Channel_14 on PC4 pin) which reads a shunt resistor between low side FET's and ground(GND).

 

Since i use pwm I was wondering if there is any method using ADC to sync the aquisition trigger on the "on state" of  the pwm signals?

 

Do i need DMA for this? since i work only with one physical adc channel

 

What is.. lets say common practice to configure ADC to capture in sync with pwm "on time"? Maybe a code reference would be also fit well.

 

Thank you

Outcomes