AnsweredAssumed Answered

STM32F413 SRAM2 through I-Code/D-Code bus.

Question asked by mendes.ari.001 on Jan 17, 2017
Latest reply on Jan 17, 2017 by mendes.ari.001

Hi,

 I want to use the STM32F413 SRAM2 to run interrupt control loop routines, as I do for CCM-SRAM of the STM32F303.

 So I need to configure the SRAM2 to be acessed through the I-Code/D-Code bus (address 0x10000000) to burst the performance.

 

I didn't figure out how to do it reading the reference manual. 

 

SRAM2 can be acessed at the address 0x20040000 or at the address 0x10000000, or I need to to some register configuration to change de SRAM2 address from 0x20040000 to 0x10000000?

 

Can I use the procedure to run an Interrupt routine at STM32F303 CCM-RAM for the F413 SRAM2?

 

Ari.

Outcomes