AnsweredAssumed Answered

STM32 Nucleo-L053R8 board: "No space left on device" on linux

Question asked by Raghavendra Kandur on Jan 16, 2017
Latest reply on Jan 16, 2017 by waclawek.jan

Hi,

 

I am downloading an elf file to STM32 Nucleo-L053R8 board.  The size of elf is given below:

text       data        bss        dec        hex    filename
54700        728       3504      58932       e634    ../mDigitalIO_ADC.elf

 

In Linux, for the very first time, the elf successfully downloaded to the target and running properly.  But next time if try to download I am facing the following issue:

 

No space left on device

 

 

If the board is disconnected and reconnected to the Linux machine the download is successful but the second time the same issue occurs.

 

But in windows, the repeated downloading to the target using simple copy commands works well and the elf runs successfully.

 

Is there any way to download the elf to Nucleo-L053R8 board without disconnect and reconnect on Linux machine without using st-link debugger instead using just 'cp' command.

 

Regards,

Raghavendra

Outcomes