AnsweredAssumed Answered

Bug Report: CUBEMX 4.18.0 no trigger selection on ADC

Question asked by frackers on Jan 12, 2017
Latest reply on Feb 9, 2017 by Jeanne Joly

Upgrading from 4.17 to 4.18 has silently removed the selection of external triggers from ADC2 on an F303RE. Not only are the selections missing from the generated code, the option in the UI is missing as well.

 

Manually patching the generated 'main.c' file fixes the problem but it means that each time I regenerate the code I have to remember to hack it.

 

I would also question the operation of the EOCSelection field as the UI allows 'ADC_EOC_SINGLE_SEQ_CONV' to be chosen but the HAL code itself says '/*!< reserved for future use */'

Outcomes