AnsweredAssumed Answered

iNemo (LSM6DS3) with external trigger

Question asked by Alan Chambers on Jan 9, 2017
Latest reply on Jan 16, 2017 by Alan Chambers

I would like to use an iNemo with an external magnetometer (i.e. Sensor Hub mode) to gather data and place acc, gyr and mag readings in the FIFO. Is it possible to have the mag drive the ODR of the iNemo with its data ready line?

 

The mag data is the most important, and it would be nice to collect data at its max ODR of 220Hz. The iNemo supports rates of 208Hz, 416Hz, and so on. I would prefer to avoid rates where I get duplicates or dropouts in the mag data.

 

Thanks.

Outcomes