AnsweredAssumed Answered

AC6 STM32 workbench broken after update

Question asked by mouser on Jan 8, 2017
Latest reply on Jan 8, 2017 by mouser

I had previously set up the STM32 workbench under Eclipse and had it working nicely with some L6474 boards on a Nucleo.

 

I recently did an upgrade from the deprecated Fedora 23 I had been using to Fedora24. This included updating to Eclipse "Neon" 4.6.1

 

I can still build the existing project code but if I try to run the debugger is fails to load gdb because it fails to find ncurses version 5 libs and I now have version 6.

 

No down grades are available to either eclipse nor ncurses.

 

What can I do to fix my development system?

 

Thanks.

Outcomes