AnsweredAssumed Answered

GPIO interrupt problem

Question asked by Denis Gottardello on Jan 4, 2017
Latest reply on Jan 5, 2017 by Denis Gottardello

Hi everybody.
I have to implement a Wiegand reader on a STM32 demo board.
Using CubeMX I have defined 2 gpios as GPIO_EXTI and now the HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) is triggered.
The problem is that the callback is triggered more than the right number of times!!!
The right number is 34 but the callback can be triggered 50, 40, 60 times!!!
Is there a way to have a right Wiegand event?

Outcomes