AnsweredAssumed Answered

make pre-calibration time shorter

Question asked by ishikawa.yu on Dec 22, 2016
Latest reply on Apr 21, 2017 by ishikawa.yu

Hi

 

I'm using multiple vl6180x devices and want them to work more quick.

However, when the second device starts in pre-calibration time of first device, the range data looks wrong.

When I set the interval more than 4ms between two devices, their range data looks correct.

So, I guess that in the case that two devices work simultaneously in their pre-calibration time, the interference occurs.

Then, I would like to ask whether I make pre-calibration time shorter than 4.3ms or skip pre-calibration phase.

I read the data sheet of vl6180X and found the pre-calibration time is fixed.

However, I want absolutely multiple vl6180x devices to work simultaneously.

Otherwise, I want them to work more quickly (less than 4ms interval). 

Is it possible?

 

Best regards

Ishikawa

Outcomes