AnsweredAssumed Answered

Problem reading or writing to NAND Flash with FSMC

Question asked by Matras.Tugrul on Dec 15, 2016
Latest reply on Jan 30, 2018 by Jeanne Joly

Hello All,

 

I am working on STM32F407ZGT6 and HY27UF081G2A NAND Flash. You can find schematics and data sheets in the attached file. I am using CubeMX to generate codes on Keil U5. You can find initialization codes below.

 

/** Perform the NAND1 memory initialization sequence*/
hnand1.Instance = FSMC_NAND_DEVICE;
/* hnand1.Init */
hnand1.Init.NandBank = FSMC_NAND_BANK2;
hnand1.Init.Waitfeature = FSMC_NAND_PCC_WAIT_FEATURE_ENABLE;
hnand1.Init.MemoryDataWidth = FSMC_NAND_PCC_MEM_BUS_WIDTH_8;
hnand1.Init.EccComputation = FSMC_NAND_ECC_DISABLE;
hnand1.Init.ECCPageSize = FSMC_NAND_ECC_PAGE_SIZE_512BYTE;
hnand1.Init.TCLRSetupTime = 0x2;
hnand1.Init.TARSetupTime = 0x2;
/* hnand1.Info */
hnand1.Info.PageSize = 0x00000800; // 2048 Bytes/Page
hnand1.Info.SpareAreaSize = 0x00000040; // 64 Bytes Spare
hnand1.Info.BlockSize = 0x00000040; // 64 Pages/Block
hnand1.Info.BlockNbr = 0x00000400; // 1024 Blocks
hnand1.Info.ZoneSize = 0x00000400; // 1024 Blocks/Zone
/* ComSpaceTiming */
ComSpaceTiming.SetupTime = 0x5;
ComSpaceTiming.WaitSetupTime = 0x3;
ComSpaceTiming.HoldSetupTime = 0x2;
ComSpaceTiming.HiZSetupTime = 0x5;
/* AttSpaceTiming */
AttSpaceTiming.SetupTime = 0x5; //0;
AttSpaceTiming.WaitSetupTime = 0x3; //2;
AttSpaceTiming.HoldSetupTime = 0x2; //1;
AttSpaceTiming.HiZSetupTime = 0x5; //4;

if (HAL_NAND_Init(&hnand1, &ComSpaceTiming, &AttSpaceTiming) != HAL_OK)
{
Error_Handler();
}

 

 

When I try to readID (HAL_NAND_Read_ID) it looks like the CPU is stuck. It doesn't go further after the first line of the command sequence. 

 

/* Send Read ID command sequence */
*(__IO uint8_t *)((uint32_t)(deviceaddress | CMD_AREA)) = NAND_CMD_READID;

(it looks like it is in an infinite loop here)
*(__IO uint8_t *)((uint32_t)(deviceaddress | ADDR_AREA)) = 0x00U;

 

 

I would appreciate it if someone help me with the issue.

 

Regards.

Tugrul

Outcomes