v.ramasubbu

About  IAP and ISP programming hardware design STM32F407

Discussion created by v.ramasubbu on Dec 16, 2016

Hi everyone..

                    I am going to use STM32F407VET (100 pin )for my design.It needs a  provision CAN,ETHERNET,SPI,USB,I2C USART interfaces and to program a flash through USART. so my doubt is other than these pins USART1 (PA9/PA10) , USART3 (PC10/PC11 or PB10/PB11) can i use (USART (TX,RX) pins) for programming a flash . if its not which pin count controller is suitable for my needs ..

 

 

                 

 

                 

 

 

 

 

Regards & Thanks ,

Ramasubbu.V.

Outcomes