AnsweredAssumed Answered

Inspite of google, unable to set up RX-interrupt on STM32F0

Question asked by garg.ajay.001 on Dec 15, 2016
Latest reply on Dec 15, 2016 by garg.ajay.001

Hi All.

 

I have a SOC, wherein a STM32F0 is connected to a modem via UART1.

The communication works "mostly" fine when AT commands/responses are exchanged synchronously, but obviously things are not stable due to overrun-issues.

 

So, I am wanting to convert to async mode.

 

Following is the relavant code :

 

 

 

void init_at_interface() { USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); USART_ITConfig(USART1, USART_IT_RXE, ENABLE) } void USART1_IRQHandler(void) { USART_SendData(USART3, (unsigned char)'>'); }

 

 

Note that UART3 is connected to putty, and is used for "debugging".

 

Finally, when I send do a USART_SendData(UART1, "\r\nAT\r\n"), I receive absolutely nothing on UART3/debug-screen (meaning that USART1_IRQHandler) is never hit.

 

What stupidity am I committing?

Outcomes