AnsweredAssumed Answered

wifi_reset Problem with IDW01M1

Question asked by Davidov.Arthur on Dec 14, 2016
Latest reply on Nov 24, 2017 by Raghuram Devanur

I'm using the STM32F411RE board with the IDW01M1 WiFi expansion module. I run some examples from en.x-cube-wifi1_firmware.zip lib.

However, all example code I run always fail during the wifi_init() --> wifi_reset() call where it just hangs in this while loop:

  while(IO_status_flag.WiFi_WIND_State.WiFiHWStarted != WIFI_TRUE)
   {
      __NOP(); //nothing to do
   }

but WiFiHWStarted never gets set to WIFI_TRUE.

Maybe i dismissed some wiring conncetions (the expantion connected via wires to eval board)?
I have JP3 set in the 1-2 position (which it is). I also have JP4 set in the 1-2 position.
I have connceted 3.3v to CN7 pins 12&14.

 

Thanks,

Outcomes