AnsweredAssumed Answered

USB baud rate

Question asked by Moamen Ayman on Dec 15, 2016
Latest reply on Dec 17, 2016 by Moamen Ayman

Hello, I'm trying to work with USB FS mode embedded in stm32f407vgt6 as device connected to PC(host), the reference manual says FS mode supports 12MHz speed and it's mentioned in the notes of CDC library (version 1.2) that "Note: In your terminal are options to set baudrate, stop bits, etc. Leave that at it is, these settings don’t care, because everything is configured by USB." I don't understand this statement, does that mean it will work directly on full speed which is 12MHz because I don't find function in CDC library to set the baud rate, I do want to work on this maximum speed but how can I configure the speed?  

Thanks in advance! 

Outcomes