AnsweredAssumed Answered

USB communication at 50Mbps using STM32

Question asked by levy.udi.001 on Dec 13, 2016

Hi all,

 

I would like to implement USB communication at 50Mbps using STM32 as a device- based on ST's existing example code.

I would like to understand if this is possible to achieve using the standard example code assuming I will use the USB HS of the controller.

 

Can I use the CDC or MSC class code examples to achieve this?

Outcomes