AnsweredAssumed Answered

STM32F two independent CAN BUS

Question asked by Khetani.Krunal.002 on Dec 12, 2016
Latest reply on May 21, 2018 by Clive One

I am new in CAN bus protocol and wanted to use two CAN channels in the STM32F as I have to receive/transmit data from/to the two different CAN bus. As per study I found that there is no master slave concept in CAN protocol but when I look at cubemx, it is configuring CAN1 as a Master and CAN2 as a Slave. In STM32F7, there are two Master CAN and one slave. What does it mean? Is it possible to transmit data using slave (CAN2)?

 

Please guide.

Outcomes