AnsweredAssumed Answered

ADC 1 problem with STM8S-Discovery

Question asked by LaserElettronicaSRL on May 26, 2015
Latest reply on Sep 12, 2017 by Mojżesz Winnetou
Hi,
I have problem with ADC1 conversions on STM8S-Discovery.
I have configured the analogic inputs following:
PB4 - AN4
PB5 - AN5
PB6 - AN6

unsigned char ADC_Config_INT ( void )
{
    
    GPIO_Init(ADC_PORT,ADC_15V_PIN, GPIO_MODE_IN_FL_NO_IT);
    GPIO_Init(ADC_PORT,ADC_CURR_PIN, GPIO_MODE_IN_FL_NO_IT);
    GPIO_Init(ADC_PORT,ADC_5V_PIN, GPIO_MODE_IN_FL_NO_IT);
 
    /* De-Init ADC1 peripheral */
  ADC1_DeInit();
    
  /* Enable EOC interrupt */
  ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE);
    
  /* Enable conversion data buffering */
  ADC1_DataBufferCmd(ENABLE);
    
  /* Enable scan mode conversion */
  ADC1_ScanModeCmd(ENABLE);

  /* Init ADC1 peripheral */
    /* ADC1 Channel 4 */
  ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_4, ADC1_PRESSEL_FCPU_D8, \
            ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL4,\
            DISABLE);
                        
    /* ADC1 Channel 5 */
  ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_5, ADC1_PRESSEL_FCPU_D8, \
            ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL5,\
            DISABLE);
                        
    /* ADC1 Channel 6 */
  ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_6, ADC1_PRESSEL_FCPU_D8, \
            ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL6,\
            DISABLE);                       
    
  /* Enable ADC1 */
  ADC1_Cmd(ENABLE);
        

    return 0;
}

the interrupt function code is:

#define ADC_SAMPLES 8
extern volatile uint16_t ValueCh4[ADC_SAMPLES];            
extern volatile uint16_t ValueCh5[ADC_SAMPLES];            
extern volatile uint16_t ValueCh6[ADC_SAMPLES];            
volatile uint8_t Index = 0;
extern uint8_t ArrayEmpty;

/**
  * @brief  ADC1 interrupt routine.
  * @param  None
  * @retval None
  */
 INTERRUPT_HANDLER(ADC1_IRQHandler, 22)
{

            if ( ADC1_GetFlagStatus(ADC1_FLAG_EOC) != RESET )
            {
                ValueCh4[Index] = ADC1_GetBufferValue(4);
                ValueCh5[Index] = ADC1_GetBufferValue(5);
                ValueCh6[Index] = ADC1_GetBufferValue(6);

                // Controlla se ho acquisito un numero sufficiente di campioni
                if( Index >= ADC_SAMPLES )
                        {
                            ArrayEmpty = 1;
                            Index = 0;
                        }    
                else{
                            Index++;
                        }
 
                
                ADC1_ClearFlag(ADC1_FLAG_EOC);
            }    

        
    return;

}

The "ADC1_GetBufferValue" function return the value correct the first time only.
If I modified the value on pin PB4 for example, continuos at read the previous value.
Any idea?
Thanks

Outcomes