AnsweredAssumed Answered

Blink all elements on LCD

Question asked by lauf.flo on Mar 13, 2015
Hey,

I want a very simple example: All elements on LCD should blink at startup(so in this very simple example: for everytime ;)

So I want to use the BlinkConfig Function from the StdLibrary... My example code:
1.LCD_GLASS_Init();
2.LCD_BlinkConfig(LCD_BlinkMode_AllSEG_AllCOM, LCD_BlinkFrequency_Div256);
3.while(1)
4.{
5.}

I'm only using the StandardLibrary. When debugging, the values of the LCD_CR1 seems to be ok, but nothing happens on the LCD... 
How to let blink all elements on the discovery-LCD with the BlinkConfig command?

Outcomes