AnsweredAssumed Answered

SPWF01Sx client- server

Question asked by max0101.max0101 on Jul 5, 2016
Latest reply on Jul 5, 2016 by max0101.max0101
Hi 
I have two SPWF01Sh device is installed between the communication method of
server
AT + S.SSIDTXT = SPWF_AP
AT + S.SCFG = wifi_priv_mode, 1
AT + S.SCFG = wifi_wep_keys [0] 7465737431
AT + S.SCFG = wifi_wep_key_lens, 05
AT + S.SCFG = wifi_mode, 3
AT & W
AT + CFUN = 1
AT + S.SOCKD = 32000, t
client
AT + S.SSIDTXT = SPWF_AP
AT + S.SCFG = wifi_priv_mode, 1
AT + S.SCFG = wifi_wpa_psk_text, test1
AT + S.SCFG = wifi_mode, 1
AT & W
AT + CFUN = 1


When wifi_priv_mode, 0 no problems if I set the type of protection
wifi_priv_mode, 1 сlien can not connect network search
+ WIND: 21: WiFi Scanning


+ WIND: 35: WiFi Scan Complete (0x0)


+ WIND: 21: WiFi Scanning


+ WIND: 35: WiFi Scan Complete (0x0)


during calibration using the command AT + S.SCAN
 BSS CC: 5D: 4E: 4D: EE: 4A CHAN: 11 RSSI: -87 SSID: 'SPWF_AP' CAPS: 0431
ustanovlinoy no WEP protection is due to petsifikatsiey miniAP or am I not right tune?

Outcomes