AnsweredAssumed Answered

AT+S.SCAN problem

Question asked by stocchi.sandro on Mar 8, 2016
Latest reply on Mar 8, 2016 by Gerardo Gallucci
Hi, 

I performed  a session of test with this spwf01 module in station mode with a router wifi.
I saw a problem that it accours sometimes during a scanning for  find 
wifi network.  




I sent a command to the module:


AT+S.SCAN


The module answer




1:      BSS C4:EA:1D:B1:CA:43 CHAN: 01 RSSI: -83 SSID: 'Telecom-29755459' CAPS: 0411 WPA WPA2 WPS 
2:      BSS D0:D4:12:A6:C0:3B CHAN: 01 RSSI: -86 SSID: 'Telecom-44482613' CAPS: 0411 WPA WPA2 WPS 
3:      BSS 98:E7:F5:49:55:67 CHAN: 01 RSSI: -84 SSID: 'WebPocket-5567' CAPS: 0411 WPA2 WPS 
4:      BSS 10:13:EE:07:5F:B5 CHAN: 06 RSSI: -89 SSID: 'Optima Italia' CAPS: 0411 WPA WPA2 
5:      BSS C4:6E:1F:F4:DB:62 CHAN: 07 RSSI: -48 SSID: 'WebPocket-1558' CAPS: 0431 WPA2 WPS 
6:      BSS 54:B8:0A:13:8D:10 CHAN: 11 RSSI: -80 SSID: 'abcpp' CAPS: 0431 WPA WPA2 WPS 


I connected the module at the sixth Network  and selected a bad password that saved in the memory of the device spwf01.


I selected a correct private mode 


AT+S.SCFG=wifi_priv_mode,2


response:OK


AT&w


response:OK


I turned on again the module and after that appeared these messages :


+WIND:1:Poweron (150410-c2e37a3-SPWF01S)


+WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc.  All rights Reserved.


+WIND:3:Watchdog Running


+WIND:0:Console active




+WIND:32:WiFi Hardware Started  


+WIND:21:WiFi Scanning


+WIND:35:WiFi Scan Complete (0x0)


+WIND:18:WiFi Join:54:B8:0A:13:8D800


+WIND:21:WiFi Scanning


+WIND:35:WiFi Scan Complete (0x0)


+WIND:19:WiFi Join:54:B8:0A:138D:10


AT+S.SCAN  (  I send a new command AT+S.SCAN but the module answer )


ERROR: Wait for Hardware Busy  




The only mode for resolve this error is change the private mode to zero 


AT+S.SCFG=wifi_priv_mode,0


response:OK


AT&w


response:OK


and restart the module.


Now if send a scan request   the module return the wifi network list correctly.


why This happens sometimes?
what is the reason?

Outcomes