AnsweredAssumed Answered

Bugreport Cube32MX 4.0 & HAL_UART_TxHalfCpltCallback

Question asked by Osto on Aug 2, 2014
Latest reply on Aug 5, 2014 by Montassar BEN ROMDHANE
Hi,

In the HAL documentation, stm32fxx_hal_uart.c & .h, I can read that in interrupt mode, the HAL_UART_TxHalfCpltCallback is called after half of tx is transfered but this is wrong.

The HAL_UART_TxHalfCpltCallback is only called if I use DMA transfers. Either is the documentation wrong or the function is not implemented to end.

Outcomes