AnsweredAssumed Answered

Need Help setting up STM32Discovery

Question asked by nanayakkara.harshana on Apr 9, 2011
Latest reply on Jun 11, 2012 by Sam
Hello there

I'm really new to this :) i was wondering if someone can help me to set up my STM32 VL Discivery.

so far I have done the following;
I'm using Vista home premium
I installed Eclipse galileo / Helios and ST link ST-LINK_gdbserver
Codesourcery Lite EABI toolchain
And i have installed the follwoing  Plugins for eclipse
 GNU Arm Development Tools
Zylin Embedded CDT

so when try to debug a code I'm getting the following two errors

"Remote communication error.  Target disconnected.: No error.
load
You can't do that when your target is `exec'
break main"

sometimes i get this

"localhost:61234: A connection attempt failed because the connected party did not properly respond after a period of time, or established connection failed because connected host has failed to respond.
load
You can't do that when your target is `exec'
break main"


if someone can help to fix this :)

thanks

Harshi

Outcomes