AnsweredAssumed Answered

UART/USART bug in STM32CubeMX V4.3 with STM32Cube V1.0

Question asked by Osto on Jul 31, 2014
Latest reply on Sep 10, 2014 by Andrew Neil
Hi,

There is a bug in STMCube when using UART/USART. When I config STM32F407VG and config UART4 and USART2 with MDK, then only stm32fxx_hal_uart is included. The stm32fxx_hal_uSart is not included and so is the config not useable. I have to add the stm32fxx_hal_usart.c manually to be able to use its functions.
See attached file which produces only UART file and not USART files.

Attachments

Outcomes