AnsweredAssumed Answered

Using two FlexPWM modules with RPC56EL70L5 (SPC56EL70L5)

Question asked by dave on Jan 14, 2016
Latest reply on Jan 21, 2016 by Erwan Y
Hi,
I am evaluating the use of RPC56EL70L5 to control two BLDC motors, using a FlexPWM module for each motor.
The datasheet of the SPC56EL70L5 states that the second FlexPWM is not connected to the pins of the package - the RPC56EL70L5 datasheet is not explicit about.
Is there a way to connect the second module (FlexPWM_1) to the output pins?
Any workaround?

Thanks, dave

Outcomes