AnsweredAssumed Answered

Spirit1 PA Configuration

Question asked by l.hcer on May 13, 2015
Latest reply on May 14, 2015 by pecorino.salvatore_g
Hi,

Which PA configuration parameters should I use in order to get the maximum output power on Spirit1 and which CWC (0 - 1.2 - 2.4 - 3.6 pF) bit field should be set for 868 MHz band?

According to the datasheet the max output power is +11dBm or +16dBm for two different test condition. Then in the registers table it is +12 dBm for the PA_LEVEL_7. This is the highest level for the highest power. Which value should be set to POWER_DBM for max output power?  I use 868MHz band with range extender. I perform the communication with GFSK_BT1 modulation at 115200 datarate. 

Best regards

Outcomes