AnsweredAssumed Answered

use rs232 uart with stm8l discovery board

Question asked by gfranck on Aug 12, 2011
Latest reply on May 14, 2013 by leckie.robert
Hi,

I would like to use the uart device of the stm8l chip on the stm8l discovery board.
I notice that uart and cristal are shared on the same pins (PA2 and PA3)

Do you think it is possible to use the uart when the stm8l is working with the 32khz oscillator or on the internal 16 Mhz internal RC ?

I don't care of the speed RS232 speed, even 300 bauds is fine for me,

Thanks,
Franck

Outcomes