AnsweredAssumed Answered

STM32CubeMx with FreeRTOS, LED, UART stuck in infinite loop

Question asked by Phua.Eugene on Jul 31, 2014
The interrupt handler is generated by CubeMx in another file.
Here is the code, no changes were made to it:

/**
* @brief This function handles EXTI Line 0 and Line 1 interrupt.
*/
void EXTI0_1_IRQHandler(void)
{
  HAL_NVIC_ClearPendingIRQ(EXTI0_1_IRQn);
   
  HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_0);
}

However, this is for the user push button. I feel the LED initialization should still be ok..

Outcomes