AnsweredAssumed Answered

LIS3DH HW or SW reset

Question asked by grunert.norbert on Oct 14, 2016
Latest reply on Oct 21, 2016 by Miroslav B
Hello,

Is there a way to manually reset the LIS3DH? In our application, VCC is coming up *very* slowly, inherent to the system. I have the suspicion that the LIS3DH occasionally does not boot correctly as it fails self-test after boot. Power-cycling it brings it back to normal. Memory reboot (CTRL5:BOOT = 1) does not help.

We have a clean reset source which takes care of the reset of the system. Is there another way to control the LIS3DH reset? There is a pin called 'RES' to be tied to GND which could stand for 'RESET' (or 'RESERVED'...).

Thanks,

Norbert

Outcomes