AnsweredAssumed Answered

SPC564B74 FlexCANs are limited to 32 Mailboxes instead of 64

Question asked by Aurelien.Leclercq on Sep 2, 2015
Latest reply on Sep 2, 2015 by Erwan Y
Hello,
I'm using SPC5Studio V3.6 and SPC564B74. The HAL drivers are limiting FlexCAN mailbox number to 32 but this CPU has 64 MB per FlexCAN.
I can change SPC5_CAN_NUM_RX_MAILBOXES and SPC5_CAN_NUM_TX_MAILBOXES définitions in mcuconf.h but this file seems not to be "patchable". It has to be changed manually every time the code is generated.
Fixes is welcome.
Aurélien

Outcomes