AnsweredAssumed Answered

Need help for STM32F4 TCP/IP connection

Question asked by k..daniel on May 8, 2014
Latest reply on May 8, 2014 by Clive One
Hey,

I´m using the STM32F407ZG from the mikroe TFT starter kit. Now I want to get an Ethernet Connection with mikroemedia shield. The Connection should work over TCP/IP and DHCP can´t be used. I´m trying the example from the libstock site but I don´t get a physical Connection at least.

I´m using the Net_Ethernet_Intern_STM32 libary from Libstock.

When I try to initialize Ethernet then the linker hung up, if I comment it out then it works like before.  Can anybody help me ?

Thanks a lot

Outcomes