AnsweredAssumed Answered

Best Practice for Using STM32Cube on Existing Project?

Question asked by Moore.Allen on Jul 31, 2014
Latest reply on Sep 10, 2014 by STM32Cube-T
I need to add USB Host (FS, MSC) capability to an existing project that's using a STM32F205 (my client wants the product to be able to read/write to a USB flash drive). Using STM32CubeMX v4.3 I created a new project, selected the FATFS and USB_HOST middleware, and the USB_OTG_FS IP, and then generated the source code. So far so good.

But is there a recommended way to integrate the resulting tree of files into an already existing project, avoiding conflicts with the existing code?

Outcomes