AnsweredAssumed Answered

Can't update wifi module via ota

Question asked by maciejowski.seth on Nov 9, 2015
Latest reply on Nov 10, 2015 by maciejowski.seth
Hey folks,
Here's what I've got:
A module with 140805-3f58d6b-SPWF01S firmware.  
I attempt to fw update to 3.4 over the air and the module downloads everything but doesn't seem to apply the firmware update to the module. Here is the transaction:

at+s.fwupdate=XXX.XXX.XXX.XXX,/SPWF01S-150410-c2e37a3-RELEASE-main.ota
.....................(many other rows of Write len 4096 -> 0xXXXXX).................
 Write len 4096 -> 0x52000
 Write len 4096 -> 0x53000
 Write len 4096 -> 0x54000
 Write len 4096 -> 0x55000
 Write len 4096 -> 0x56000
 Write len 4096 -> 0x57000
 Write len 4096 -> 0x58000
 Write len 4096 -> 0x59000
 Write len 4096 -> 0x5A000
 Write len 4096 -> 0x5B000
 Write len 4096 -> 0x5C000
 Write len 4096 -> 0x5D000
 Write len 4096 -> 0x5E000
 Write len 4096 -> 0x5F000
 Write len 1812 -> 0x60000 (final)
 Wrote 390932 bytes
 Complete!  Update will be applied on next reboot. (at+cfun=1)
 at+cfun=1
+WIND:2:Reset
+WIND:32:WiFi Hardware Started
+WIND:21:WiFi Scanning
+WIND:35:WiFi Scan Complete (0x0)
+WIND:19:WiFi Join:00:30:44:14:B6:F3
+WIND:25:WiFi Association with 'WifiTestJig' successful
+WIND:51:WPA Handshake Complete
+WIND:24:WiFi Up:192.168.210.78
at+s.sts
# Status & Statistics:
#  version = 140805-3f58d6b-SPWF01S 

Any suggestions?

Outcomes