AnsweredAssumed Answered

details are needed for HAL_LE_TX_TEST_PACKET_NUMBER

Question asked by shao.hui on Apr 17, 2015
Latest reply on May 11, 2015 by Marchese.Graziella
In AN4494, Bring up BlueNRG app note, both Chapter 8 and 9 mention that

 

Send a further command to determine the number of packets sent by the Tx board: HAL_LE_TX_TEST_PACKET_NUMBER

What is the LE command above? Where can I find relevant code for it? I need it to get the actual number of TX packet sent for board RF tuning. I have code from DK1.6.0 for

 

HCI_LE_TRANSMITTER_TEST,

and

 

HCI_LE_TEST_END .


Thanks!

Hui

Outcomes