AnsweredAssumed Answered

usb library on windows 7 (does not work)

Question asked by pataky.ed on May 1, 2014
Latest reply on May 16, 2014 by rowse.chris
I am trying to use the usb library found here:  
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257882#

I am on windows 7, I am using the port207z board here with the STM32f207z: 
http://www.wvshare.com/product/Port207Z.htm

I load the example under: 
\USB\stm32_f105-07_f2_f4_usb-host-device_lib\STM32_USB-Host-Device_Lib_V2.1.0\Project\USB_Device_Examples\VCP

or 

\USB\stm32_f105-07_f2_f4_usb-host-device_lib\STM32_USB-Host-Device_Lib_V2.1.0\Project\USB_Device_Examples\HID

In both cases, windows 7 cannot recognize the device, and even if install the driver it does not work .. i tried downloading some free usb trace software and it said enumeration failed ... 

ST told me the HID should work without needing to install any driver .. 

Has anyone gotten this to work on windows 7?

Outcomes