AnsweredAssumed Answered

Where do basic System Debug setting happen using STM32Cube

Question asked by aiyer.kartik on Apr 30, 2014
Latest reply on Apr 30, 2014 by Clive One
I'm working with a project generated by STM32CubeMX. I can see all the generated code that enables the various IPs and all the pin configuration. However, I can't locate where GPIOs are set to be used for SWD/SWO. I can see in CubeMX that PB3, PA13 and PA14 are setup for debug but I don't see this specifcally in the code. I'm asking because, when I try to get SWO output from the demonstration project, I get nothing. It leads me to believe that perhaps the BSP in the demo project does not enable the SWO pin and I wanted to find out where this happens. Any help is appreciated.

Regards
Kartik

Outcomes