AnsweredAssumed Answered

Debuging .bin file

Question asked by mr on Nov 28, 2016
Latest reply on Nov 28, 2016 by Clive One
Hello,
I am using eclipse with a Nucleo F103 and OpenOCD (or alternativly TrueStudio) and would like to do the following. 
I have a .bin file without the sourcecode. Now I would like to step through the disassembly to see where it jumps to in the code. I am not reverse engineering. Its just two bootloaders and the actual code. I have the source to one Bootloader nut not the other. So I just want to see what addresses the combined code jumps through. I dont have any other options. I can only flash the first bootloader, then with that falsh the rest and read back the binary file. This read file I would like to step through. Is this possible?

Outcomes