AnsweredAssumed Answered

Hard to track down the actual cause.

Question asked by Md Mubdiul Hasan on Nov 9, 2016
Latest reply on Dec 19, 2016 by Kraal
Hi,

In the project properties setting, I am using arm-none-eabi-gcc toolchain.
This time toolchain is Ac6 STM32 MCU GCC and builder CDT internal.

Problem is if I add h files in HAL library that error log suggest me to do, it solved and if I build project again it shows the problem in CMSIS include H files. icon_redface.gif 

Such as, 

1. C:\STM32_toolchain\common\Drivers\CMSIS\Device\ST\STM32F0xx\Include/stm32f0xx.h:187:3: error: declaration for parameter 'FunctionalState' but no such parameter
} FunctionalState;
^
..\inc\Src\stm32f0xx_hal_flash_ex.c:990:1: error: expected '{' at end of input
}
^
..\inc\Src\stm32f0xx_hal_flash_ex.c:990:1: warning: control reaches end of non-void function [-Wreturn-type]
}
^


APIs, Headers,state machine files are exists in Project branch, but why the compiler showing errors in H files of driver ?

Looking at  C code structure related reason, yes I found some style of C coding in CMSIS h files is different.

 what should I do now?


1. CDT does not showing errors of my main files, there was a return type problem, I solved it.

3. I think compiler is compiling all files listed in project branch , do you want me to remove some of the files from project folder, is it repeating again as I include paths from C driver?

4. Is there any setting for which only compile my c file?

5. Do you believe, updated version of Java/gcc/Eclipse is needed ?

I am using this HAL driver STM32Cube_FW_F0_V1.6.0 downloaded from STM website.


Hope you will give me some good suggestions.

Regards
HASAN



Outcomes