AnsweredAssumed Answered

Looking for USB HID project example that receives command from PC then display LED?

Question asked by vu.andy on Oct 11, 2016
Latest reply on Oct 18, 2016 by vu.andy
I am looking for an USB HID example that the firmware would receives for example a command from the PC then based on the input command, would display a few LED.
Currently there are a few examples from STM but it seems like only a one way communication in which the mouse would SendReport() in a while() loop.
But I am looking for an example in which the firmware would receive various commands from the PC then based on that, decides what to do in a 2-way communication.
Thanks.

Outcomes