AnsweredAssumed Answered

STM32F103 resetting

Question asked by Nayani.Partha on Oct 10, 2016
Latest reply on Oct 10, 2016 by FTITI.Walid
Hi,
I have an STM32F103RC8 controller board. I have two LEDs connected to two port bits. When I load a using flash loader demo program to toggle the LEDs the program works for a few seconds and the controller resets. If I put the boot 0 pin to boot from application the controller resets much faster. The program is very simple. Initialize GPIO port bits (only those connected to LEDs) and a while loop with a delay routine. What could be wrong? I am sure there is nothing in the program.  Thanks for your time and help.

Outcomes