AnsweredAssumed Answered

I/O Mirroring

Question asked by wilczewski.jeffrey on Sep 26, 2016
Latest reply on Sep 24, 2017 by Code Wrangler
I need to simply capture an input level and then output the same logic level as soon as possible on another pin.

This can be simply done with EXTI, but I was wondering if there is a passive peripheral based solution that could be done without software intervention.

I was wondering if one of the TIMERs could be re-purposed this way or some other peripheral?

Outcomes