AnsweredAssumed Answered

ETH DMA stuck in "waiting for status"

Question asked by danicek.jiri.001 on Sep 21, 2016
Latest reply on Sep 26, 2016 by danicek.jiri.001
Hello.
I'm working on a project, running on STM32F427IIH6, which uses FreeRTOS 6.1 and LwIP 2.0. There are several TCP clients and TCP/UDP servers and it's running with no issues. But after adding UDP client,
low_level_output occassionally fails at very first ARP packet, involved by lwip_getaddrinfo called by the UDP client. If it doesn't occur at start, whole system can run "forever".


Settings (state of registers just before first write):

MACCR == 0x0000800C // Rx and Tx enabled
MACFFR == 0x00000040 // PCF == 1
MACFCR == 0x00000080 // Zero quanta disabled
All other MAC registers except of MII and MAC address registers are zero.

DMABMR == 0x02C16080 // 32b long, address aligned, fixed burst; 2:1 Rx:Tx priority; enhanced descriptors
DMAOMR == 0x02202006 // Both Rx and Tx are started, store and forward mode. OSF mode used for Tx
DMAIER == 0x00010040 // Only Rx interrupt and summary enabled
DMASR == 0x00660004 // Rx is waiting for data, Tx is suspended and waiting for send command
Descriptor and buffer address registers have proper values, other registers are zero

I use LAN8720Ai connected via RMII and its' registers don't change since this time.

I use 5 Tx chained descriptors, all of them have set TCH bit in word 0 and filled both pointers, everything else is 0.

Success: 5 frames sent, ETS bit in DMASR is set, first 2 descriptors have set FS and LS bits and data length. Nothing else changed.

Fail (differences to success in bold): No frame sent, ETS bit in DMASR is set, TBUS is reset and TPS has value of 2, which means, that Tx DMA FSM is "Running, waiting for status". All 5 descriptors have set FS, LS and OWN bits and data length. DMACHTDR and DMACHTBAR now point at second descriptor and its' buffer.

DMA doesn't send data to MAC for some reason and when sw tries to send TX_DESC_NUM + 1 frames, I get the error. What's the "status", which is DMA "waiting for"? I haven't found anything about it in the reference manual.

Outcomes