AnsweredAssumed Answered

STM32F4 not fully programable

Question asked by Lukasz Przenioslo on Sep 19, 2016
Latest reply on Sep 20, 2016 by Clive One
Hello there,
I have a problem with programming STM32F4 device. My Jlink probe correctly sees the device over SWD but it cannot erase nor program it however- This is the Jlink command prompt when trying to erase:

https://pastebin.com/6S4KKFAZ

Some facts about the enviroment that might help resolve the issue:
- I am able to program the same MCU on a different board with the same code.
- I am able to connect with the device using Segger Jlink device, but I am not able to erase or program.
- The device stopped working after about 2 h of proper work. The program stopped and I reset the power. After that I have the current problem...
- I have checked the voltage on the device (it is also visible in the Jlink command prompts) and it is within proper range.
- I have resoldered another STM32F407 MCU to make sure the MCU is not broken.

What could be the case of this situation? If this might be hardware related, what could be the case? I believe that if the ribbon cable connecting the board with the debbuger was faulty, I wouldnt be able to connect at all?
I would really appreciate all help, I am getting out of ideas...

Outcomes