AnsweredAssumed Answered

Setting Ethernet: DHCP & MAC address - STM32F746NG

Question asked by brooks.peter.001 on Sep 5, 2016
Latest reply on Sep 5, 2016 by ForumSTM32.ForumSTM3
As the title says, I'm wanting to set the Ethernet chip to enable DHCP and set its MAC address.

As I understand it - and I may well be wrong, so I'd be grateful for correction if I am - the chip manages the DHCP negotiations, all it needs is to be enabled to do this, and, of course, to have a MAC address set.

I'm using Ada, so I don't have access to the C-library that does this - which is why I need to have more detail of how it works.

I believe, again, correct me if I'm wrong, that I need to set a register, with the correct bit and correct address. I don't know which register I need to set.

What is the correct register - or, even better, where is there documentation that gives the address of the register, and the register contents?

Outcomes