AnsweredAssumed Answered

Nucleo f429zi after st-link removal

Question asked by zyx.zxy on Aug 29, 2016
Latest reply on Sep 22, 2016 by FTITI.Walid
Hello,
I have a following problem, I have a Nucleo f429zi board and after ST-link removal I am unable to run code on it. I've chcecked the solder bridges, I'm using SWO - the debbuging seems to be fine, the cpu is stuck on "  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)" I've even tried soldering the oscillator and caps to the "x3" space as the MCO is gone, since I removed the ST-link.

Here is the configuration (it is the default one):

http://pastebin.com/KbhfhiSk

I'm trying to run a simplest code - toggle the LED. Now, i don't know if the problem is related to hardware or something is wrong with my SW4stm32. Is this a problem with the HSE? If I download blinking LED *.bin from the Mbed platform and flash it to the board it starts up fine... maybe it is using only LSE? Please help, thanks in advance.

Outcomes