AnsweredAssumed Answered

Linking Binary File art_of_gard_448K.bin

Question asked by s_poggie on Jul 22, 2016
Latest reply on Jul 22, 2016 by waclawek.jan
Hi
I am having trouble to link a binary file for an STM32F4 Discovery project.
The Media File art_of_gard_448K.bin should be linked at the memory position


/* Audio file size and start address are defined here since the Audio file is 
   stored in Flash memory as a constant table of 16-bit data */
#define AUDIO_FILE_SIZE               0x70000
#define AUDIO_FILE_ADDRESS            0x08080000   /* Audio file address */  
  

Do I need to adopt my linker /ld script manually or is there a way to set this in TrueStudio? 
I can not see any settings in the sample project, that would reflect this, also have compared ld files of my project and the sample project. 
Please support
Thanks 
Sascha 

Outcomes