AnsweredAssumed Answered

STM32L4xx HAL_CAN_Transmit_IT() enables interrupt before transmission

Question asked by Meise_Reckefuss.Dirk on Jul 13, 2016
Latest reply on Jul 14, 2016 by ForumSTM32.ForumSTM3
Hello,

the HAL function HAL_CAN_Transmit_IT() enables the Transmit mailbox empty Interrupt before the requesting transmission.
At least if I run the CAN bus wit 1Mbit the mailbox empty interrupt is triggered before the new frame is send.
I read abaut this problem in this forum before but also new HAL drivers are delivered with the same bug!

Outcomes